Hi, We fixed the issue. Why the uboot no show the CPU information and Uboot version (such like below information.)?
U-Boot 2018.03-imx_v2018.03_4.14.78_1.0.0_ga+g0ec2a01 (May 05 2018 - 15:16:44 +0300)
CPU: Freescale i.MX6UL rev1.1 528 MHz (running at 396 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 45C
Reset cause: POR
Board: MX6UL 14x14 EVK
I2C: ready
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment