Hi,
I have iMX6 board based on SabreLite, but it has the folloowing configuration
RAM : 4*256MB, 64 bit and NAND Flash.
I used mx6q_sabresd_iram_config to create UBOOT for internal RAM, it works fine.
But My external RAM, it is failing..I am using Manufacturing Tool to load the image, it is successfully loading the image
-----------------------
loading binary file(u-boot.bin) to 27800000, skip=0, fsize=2c3f8 type=aa
<<<181240, 181240 bytes>>>
jumping to 0x27800400
----------------------------
But I don't see any serial port messages..I have to suspect my RAM Configuration, I have the following questions.
1) My board is based on SAbrelite, shall I use default flash_header.S (board/freescale/mx6q_sabrelite)?
2) In sabrelite , the booting is from NOR to RAM..is this routing I need to change for my board?
Thanks,
Regards,
Kotteeswaran G S
Kotteeswaran
This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.
Thanks,
Yixing
Hi,
Any Reply?
My System.map shows that :
27800400 t ivt_header
27800404 t app_code_jump_v
27800408 t reserv1
2780040c t dcd_ptr
27800410 t boot_data_ptr
27800414 t self_ptr
so it has proper value..only my doubt is is there anything wrong with flash_header.s file settings.
How can I correct it?
Thanks,
Regards,
Kotteeswaran G S
Kotteeswaran
We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing
Kotteeswaran
We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing