UART4 can't receive data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART4 can't receive data

801 Views
pierre-olivierh
Contributor III

Hello

I'm currently trying to receive data throught UART4, but it does not work. I can send data (on iMX6 with echo -en "hello" > /dev/ttymxc3) and it works, but when I do cat /dev/ttymxc3, I receive nothing from the host PC. I probed the RX pin, the data is correct.

This is my configuration :

pinctrl_uart4: uart4grp {
fsl,pins = <
         MX6QDL_PAD_KEY_COL0__UART4_TX_DATA 0x1b0b1
         MX6QDL_PAD_KEY_ROW0__UART4_RX_DATA 0x1b0b1
   >;
};

&uart4 {
      pinctrl-names = "default";
      pinctrl-0 = <&pinctrl_uart4>;
      status = "okay";
};

The registers for the Daisy chain seems to be set rightly:

IOMUXC_SW_MUX_CTL_PAD_KEY_COL0:0x020e01f8 =0x00000004

IOMUXC_SW_MUX_CTL_PAD_KEY_ROW0:0x020e01fc =0x00000004

IOMUXC_UART4_UART_RX_DATA_SELECT_INPUT:0x020e0938 =0x00000001

You will find attached two images, with the data on TX (in yellow) and RX (in blue), the data is decoded for more visibility. The sent data is correct, the received data also, but not displayed in linux  so I think there is an error somewhere.

I'm on iMX6Q, Kernel 3.14.38.

Best Regards,

Pierre-Olivier

Labels (1)
Tags (2)
1 Reply

647 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pierre-Olivier

uart4 is used on sabre-ai board, imx6qdl-sabreauto.dtsi
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6qdl-sabreauto...

Schematics (5)
Design files for i.MX 6Quad and i.MX 6DualLite CPU1 Cards
Design files for Base Board (REV E)

http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply