UART's with CTS ONLY to drive RS485 driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART's with CTS ONLY to drive RS485 driver

3,995 Views
ramgopalkota
Contributor I

Hi 

I have a question on Hardware and Linux driver usage.

We are using iMX6UL CPU ( ) and want to use all the 8 CPU's.

We are reserving UART1 as debug console.

For rest of the UARTs (7 numbers) we want to drive a RS485 driver (ADM2687EBRIZ) direction control via CTS/RTS ?

As per the documentation I am not clear if I need to reserve RTS and CTS lines ? or just CTS lines is good enough ?

If CTS line is good enough then how to configure in the dts file ? All the DTS examples are using both the lines.

e.g. used is UART2 

Configure in the DTS to have 3 Lines Tx,Rx,CTS  (DCE Mode)

&uart2 {

pinctrl-names = "default";

pinctrl-0 = <&pinctrl_uart2>;

uart-has-rtscts;

status = "okay";

};

In the imx.c driver , I see that if "have_rtsgpio" is not set then the toggling will not happen and the comment says RTS is required.The comment is based on UART mode in DTE as RTS is output in DTE only and input in DCE mode.

/* RTS is required to control the transmitter */

if (!sport->have_rtscts && !sport->have_rtsgpio)

     rs485conf->flags &= ~SER_RS485_ENABLED;

In the above structure , do I need to enable have_rtsgpio ? 

pinctrl_uart2: uart2grp {

fsl,pins =

< MX6UL_PAD_UART2_TX_DATA__UART2_DCE_TX 0x1b0b1

MX6UL_PAD_UART2_RX_DATA__UART2_DCE_RX 0x1b0b1

MX6UL_PAD_UART3_TX_DATA__UART2_DCE_CTS 0x1b0b1 >;

};

In the above structure do I have to have RTS line also ?

Please correct me and help me with correct pins and dts structures.

Labels (1)
0 Kudos
7 Replies

2,285 Views
analogicstechin
Contributor III

i hope u are  solved the issue Ramgopal Kota,please give suggestion way you solved ,same requirement i have in i.MX6ull  

Thanks in Advance.

0 Kudos

2,285 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ramgopal

from sect.64.7.1 Generalities i.MX6DQ Reference Manual :

The CTS_B pin can be used to control RS-485 output driver outside the chip.

so it is sufficient for RS485. Unused pin can be used for other purposes, comment

it in pinctrl_uart.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

2,285 Views
ramgopalkota
Contributor I

Hi,

We dont want to use RS485 9-bit mode. We want to use the normal UART mode

with CTS_B to control the RS485 driver.

If we dont use 9-bit mode, can we still drive CTS_B with linux.

BTW we are using iMX6UL and we are referring to reference manual (Document

Number: IMX6ULRM Rev. 1, 04/2016) and referring "53.7.1 Generalities".

Ramgopal Kota

On Fri, Jun 16, 2017 at 3:41 PM, igorpadykov <admin@community.nxp.com>

0 Kudos

2,285 Views
pyraohms
Contributor III

I am in need of information about how to do this too!

0 Kudos

2,285 Views
igorpadykov
NXP Employee
NXP Employee

yes, one can still drive CTS_B with linux even dont use 9-bit mode.

~igor

0 Kudos

2,285 Views
pyraohms
Contributor III

Does the UART's use the CTS pin by default (on imx6ul EVK)?

0 Kudos

2,285 Views
igorpadykov
NXP Employee
NXP Employee

you can check it on schematic

Schematics (1)
MCIMX6UL-EVK_DESIGNFILES
Design files, including hardware schematics, Gerbers, and OrCAD files. (REV 0)
http://www.nxp.com/products/sensors/gyroscopes/i.mx6ultralite-evaluation-kit:MCIMX6UL-EVK?fpsp=1&tab...

Best regards
igor

0 Kudos