Hi,
Kindly help me, which UART port is used for debugging in IMX7 (Part number # MCIMX7D7DVK10SC)
Thanks & Regards,
Logesh
Hello,
On iMX7DSABRESD board J11 connector is used for Debug UART (via USB).
According to board schematic: Debug UART1 is intended for Cortex-A7;
Debug UART2 for Cortex-M4.
NXP BSP(s) uses such approach, but customers can use any available UART ports
(and pins) for their applications, assuming BSP modification, if needed.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Also Kindly suggest shall we use any of below UART ports for debugging,
1. UART1 (Pin# D16 & D7)
2. UART2 (Pin# G28 & D20)
If we are not able to use the above ports for debugging kindly request you to provide correct the UART port ID with pin numbers.
Thanks & Regards
Logesh