U-boot-v2012.10 failing prep step

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-boot-v2012.10 failing prep step

2,060件の閲覧回数
mercyyuen
Contributor II

I'm using a mx6q_sabresd board for my development.  Right now my ltib is configured to use uboot-v2009.08.


I wanted to try the new uboot version 2012.10.  I found this articleLinux Fast Boot on i.MX6Q Board: Building Steps and tried to follow it.


1. Downloaded u-boot-2012.10.tar.bz2 from Index of /pub/u-boot

2. Placed this file into ../ltib/rpm/sources.

3. Created copy of u-boot-v2009.08.spec.in renamed it u-boot-v2012.10.spec.in ../ltib/config/platform/imx.

4. Updated the content of u-boot-v2012.10.spec.in to be

Version    : 2012.10
Release   

: imx_3.0.35_13.01.00

5. I selected mx6qsabresd as my hardware

6. I selected u-boot v2012.10 as my u-boot version.

7. From the command line I typed ./ltib -m prep -u u-boot

I get the error:

Try u-boot-v2012.10-imx_3.0.35_13.01.00.tar.bz2.md5 from the GPP

http://bitshrine.org/gpp/u-boot-v2012.10-imx_3.0.35_13.01.00.tar.bz2.md5:

12:09:16 ERROR 404: Not Found.

Try u-boot-v2012.10-imx_3.0.35_13.01.00.tar.bz2 from the GPP

http://bitshrine.org/gpp/u-boot-v2012.10-imx_3.0.35_13.01.00.tar.bz2:

12:09:17 ERROR 404: Not Found.

Can't get: u-boot-v2012.10-imx_3.0.35_13.01.00.tar.bz2 at ./ltib line 802.

f_prep() returned an error, exiting

traceback:

main:572

Can someone please tell me what I'm doing wrong?  I feel like I must be missing a very basic step.

ラベル(3)
6 返答(返信)

1,037件の閲覧回数
YixingKong
Senior Contributor IV

Mercy

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 件の賞賛

1,037件の閲覧回数
YixingKong
Senior Contributor IV

Mercy

We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛

1,037件の閲覧回数
YixingKong
Senior Contributor IV

Mercy

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛

1,037件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Just build U-boot manually without LTIB. This is make things much easier.

0 件の賞賛

1,037件の閲覧回数
GraceH
Senior Contributor II

You need rename  u-boot-2012.10.tar.bz2 to  u-boot-v2012.10-imx_3.0.35_13.01.00.tar.bz2 in folder  ltib/rpm/SOURCES

and run  md5sum u-boot-v2012.10-imx_3.0.35_13.01.00.tar.bz2 > md5sum u-boot-v2012.10-imx_3.0.35_13.01.00.tar.bz2.md5

Grace

0 件の賞賛

1,037件の閲覧回数
mercyyuen
Contributor II

Hi Grace,

I tried your suggestion. I renamed the file, and then from ~/ltib/rpm/SOURCES I ran the command you suggested.

I got the following error.

md5sum: u-boot-v2012.10-imx_3.0.35_13.01.00.tar.bz2.md5: No such file or directory.

Please advise!

Mercy

0 件の賞賛