U-boot hab_status indicate warnings but no events are displayed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-boot hab_status indicate warnings but no events are displayed

4,676件の閲覧回数
ollesandberg
Contributor I

We're trying to implement secure boot through HAB here. We have signed the SPL/U-boot image through cst and burnt the fuses corresponding to the public key. Now when testing for HAB events with the u-boot command 'hab_status' it displays the following:

u-boot=> hab_status
Secure boot disabled

HAB Configuration: 0xf0, HAB State: 0x66‍‍‍‍‍‍‍‍‍‍

Missing in the output is the print 'No HAB Events Found!', but no HAB events are obviously displayed either.

Further debugging shows that the u-boot function 'hab_rvt_report_status()' returns HAB_WARNING (0x69).

So question is, what does this error/warning indicate, what might be wrong with our setup?

BR, Olle

ラベル(3)
タグ(3)
0 件の賞賛
返信
8 返答(返信)

3,965件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Olle

seems it is described in RNG-self-test-patch on

https://portland.source.codeaurora.org/patches/external/imxsupport/uboot-imx/imx_v2016.03_4.1.15_2.0... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,965件の閲覧回数
ollesandberg
Contributor I

Hi Igor,

Do I understand it correctly that this is a bug in boot ROM and not caused by our setup?

The patch mentions iMX6, but it affects iMX8 also?

/Olle

0 件の賞賛
返信

3,965件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Olle

 

yes this is correct understanding.

iMX8 are not affected.

 

Best regards
igor

0 件の賞賛
返信

3,965件の閲覧回数
ollesandberg
Contributor I

Hi Igor,

We're on iMX8M so then this patch is irrelevant for our potential error I guess.

Any other idea what might be causing the warning from hab_rvt_report_status()?

Is it a problem or can it be ignored, that is - if we close the device will it still boot?

BR,

Olle

0 件の賞賛
返信

3,965件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Olle

 

sorry I missed that it is i.MX8M.
In general i.MX8M secure boot is not officially supported yet
and there is no documentation for it (only some preliminary codes).
Suggest to proceed with Professional Services
As general suggestion one can try nxp uboot from below link
and latest chip revision with suffix "B", rev.1.1.

3,965件の閲覧回数
ollesandberg
Contributor I

Is there any plan for when secure boot will be officially supported by NXP?

BR, Olle

0 件の賞賛
返信

3,965件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Olle

I think such app note will be published, unfortunately I am not aware of date.

Best regards
igor

0 件の賞賛
返信

3,938件の閲覧回数
jeremy_sauget
Contributor I

Hi,

I just found this thread while working on secure boot for imx8m evkb board.

Is secure boot supposed to be supported now ? If it is, could you please let met know the version of the BSP to use in this case. (I am trying to use it but I without success for now and looking at the code in U-Boot / ATF, I have the feeling that it is not fully supported yet but maybe I am not using the correct version of the BSP).

Best regards,

 

0 件の賞賛
返信