U-boot : NAND SPL for IMX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-boot : NAND SPL for IMX6ULL

968 Views
ge73for
Contributor I

Hello,

I am trying to build SPL to boot from NAND for IMX6ULL processor. So far i am able to build the SPL but when I flash it to NAND , it does not seem to work.

Has anyone tried this and was it successfull ?

Thank you.

Tags (4)
0 Kudos
1 Reply

903 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kavya

mx6ul_14x14_evk_spl_defconfig is not officially supported in nxp bsps, however one can check

[U-Boot] mx6ulevk: Add support for SDP boot in SPL target - Patchwork 

Standalone boot (XUELK) - DAVE Developer's Wiki 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos