U-boot Can't Access NAND on QSB based Customized Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-boot Can't Access NAND on QSB based Customized Board

2,132件の閲覧回数
HuiShao
Contributor I

Hi-

 

On a QSB based design, I have problem accessing NAND from u-boot command line.

 

NAND chip:

MT29F2G08ABBEAH4

• Single-level cell (SLC) technology

• Organization

– Page size x8: 2112 bytes (2048 + 64 bytes)

– Page size x16: 1056 words (1024 + 32 words)

– Block size: 64 pages (128K + 4K bytes)

– Plane size: 2 planes x 1024 blocks per plane

– Device size: 2Gb: 2048 blocks

 

iMX53 I/F:

PATA, WP# is tied to ground via 4k7, R/B# is pulled up to 1V8 via 4k7.

 

 

 

U-boot patched:

Patched u-boot source code by patches #0170-#0174.

 

In addition, I added the nand_device_info entry of my NAND chip (0x2c/0xaa) to table_type_7[] table in /drivers/mtd/nand/nand_device_info.c:

{
.end_of_table = false,
.manufacturer_code = 0x2c,
.device_code = 0xaa,
.cell_technology = NAND_DEVICE_CELL_TECH_SLC,
.chip_size_in_bytes = 256LL*SZ_1M,
.block_size_in_pages = 64,
.page_total_size_in_bytes = 2*SZ_1K + 64,
.ecc_strength_in_bits = 4,
.ecc_size_in_bytes = 512,
.data_setup_in_ns = 10,
.data_hold_in_ns = 5,
.address_setup_in_ns = 10,
.gpmi_sample_delay_in_ns = 6,
.tREA_in_ns = -1,
.tRLOH_in_ns = -1,
.tRHOH_in_ns = -1,
"MT29F2G08",
},

 

After bootup from SD card, I got:

MX53-CSSU U-Boot > nand device

Device 0: NAND 256MiB 1,8V 8-bit, sector size 128 KiB

 

However, I got following errors:

MX53-CSSU U-Boot > nand erase 0x20000 0x20000

NAND erase: device 0 offset 0x20000, size 0x20000

NAND 256MiB 1,8V 8-bit: MTD Erase failure: -5

OK

 

MX53-CSSU U-Boot > nand write 0xf8006000 0x0 0x20000

NAND write: device 0 offset 0x0, size 0x20000

nand_do_write_ops: Device is write protected

NAND write to offset 0 failed -5

0 bytes written: ERROR

 

MX53-CSSU U-Boot > nand read 0xf8006000 0x0 0x20000

NAND read: device 0 offset 0x0, size 0x20000

UnCorrectable RS-ECC Error

UnCorrectable RS-ECC Error

UnCorrectable RS-ECC Error

UnCorrectable RS-ECC Error

...

UnCorrectable RS-ECC Error

131072 bytes read: OK

 

Can anybody offer some hints on the problems above?

 

Thanks!


 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,301件の閲覧回数
HuiShao
Contributor I

Hi Johan

 

Yes we are using 1V8 version.

 

I tried removing 4k7 resistor from WP# but it doesn't seem to work either.

 

thanks and regards,

 

Hui

0 件の賞賛
返信

1,301件の閲覧回数
jomeke
Contributor II

Hallo,
I made also a design with the Imx537 and two nand flash 29F16G08 connected to the PATA lines.
I didn't place a pull up resistor on the WP line and it works fine.
The Bootloader starts from flash, UBOOT and Linux are also working fine.
My NAND flash works on 3V3, are you using the 1V8 version ?

Best regards

Johan

0 件の賞賛
返信