U-Boot on iMX6ULL with Linux: Which branch should we use?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-Boot on iMX6ULL with Linux: Which branch should we use?

1,483件の閲覧回数
simon_willis
Contributor II

Hi All, 

We are in the process of bringing up a new iMX6ULL board. We initially aimed to use Windows 10 IoT Core and therefore started with the relevant BSP. We got the device booting, but we've now changed our requirements and will be using Linux instead. We noticed that there are numerous branches on codeaurora. It looks like it's been 2 years since a  commit to the master branch. Therefore, which branch should we be using?

Cheers,

Simon

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,469件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello simon_willis,

See below, please!

----------------------------

Yes, it is no problem to use L5.4.24_2.1.0.

1. Downloading linux document.

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

--Supporting Information (42)

     ---- L5.4.24_2.1.0_LINUX_DOCS

1,477件の閲覧回数
simon_willis
Contributor II

Also can anyone explain how the branch naming on CodeAurora works? We are guessing it's 

<uboot-version>_<linux kernel version>_<some other version number>
 
0 件の賞賛
返信