U-Boot environment variables from MfgTool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-Boot environment variables from MfgTool

ソリューションへジャンプ
4,084件の閲覧回数
kasperholtze
Contributor I

Hello,

Is it possible to set U-Boot environment variables using MfgTool? If so, how?

Thanks,

Kasper Holtze

ラベル(1)
タグ(2)
1 解決策
2,617件の閲覧回数
raymondwang
Senior Contributor I

You can create your env binary and download to flash via MFG tool.

FYI.

mkenvimage: a tool to generate a U-Boot environment binary image

元の投稿で解決策を見る

4 返答(返信)
2,617件の閲覧回数
LeonardoSandova
Specialist I

nice tool.

There are also U-boot scripts, quite useful to fetch and execute the same set of instructions in multiple boards. I have not touch this link for a long time, but you may start with this

Running a Script in U-boot

0 件の賞賛
返信
2,618件の閲覧回数
raymondwang
Senior Contributor I

You can create your env binary and download to flash via MFG tool.

FYI.

mkenvimage: a tool to generate a U-Boot environment binary image

2,617件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi raymond,

It's really helpful information from you ~~

Thanks.

Best Regards,

Dan

0 件の賞賛
返信
2,617件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Kasper,

It can not support setting U-Boot environment variables, but only can download u-boot, uImage and fs to flash. It's a download tool.

Best Regards

Dan