[U-Boot] Is Atheros AR8033 compatible with AR8031 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[U-Boot] Is Atheros AR8033 compatible with AR8031 ?

Jump to solution
3,769 Views
charleshuang
Senior Contributor II

Hi,

The ethernet PHY of my new-board is AR8033, and I use the same u-boot-imx.bin to test the new-board and SabreSD by following commands,

setenv ethaddr 00:04:9f:02:b7:fb
setenv ipaddr 192.168.203.14
ping 192.168.203.203

The network function works well for the SabreSD, but the network function does not work for the new-board, following message shows up continuously...

ARP Retry count exceeded; starting again

For the SabreSD , the following u-boot message shows up

Net: FEC [PRIME]

For the new-board, the following u-boot message shows up

Net: Phy not found

PHY reset timed out

FEC [PRIME]

but the command "mii dump" still works, the following message is identical with SabreSD's

0.     (ffff)                 -- PHY control register --

  (8000:8000) 0.15    =     1    reset

  (4000:4000) 0.14    =     1    loopback

  (2040:2040) 0. 6,13 =   b11    speed selection = 10 Mbps

  (1000:1000) 0.12    =     1    A/N enable

  (0800:0800) 0.11    =     1    power-down

  (0400:0400) 0.10    =     1    isolate

  (0200:0200) 0. 9    =     1    restart A/N

  (0100:0100) 0. 8    =     1    duplex = full

  (0080:0080) 0. 7    =     1    collision test enable

  (003f:003f) 0. 5- 0 =    63    (reserved)

Is there any idea ?

Labels (2)
0 Kudos
1 Solution
1,821 Views
igorpadykov
NXP Employee
NXP Employee

Hi charles

as reported below ar8031 driver does not work with ar8033

[U-Boot] [PATCH] phylib: update atheros ar803x phy

One can check if ar8033 ouputs a 125MHz and hints below

Ethernet PHY not found - u-boot migration

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
1,822 Views
igorpadykov
NXP Employee
NXP Employee

Hi charles

as reported below ar8031 driver does not work with ar8033

[U-Boot] [PATCH] phylib: update atheros ar803x phy

One can check if ar8033 ouputs a 125MHz and hints below

Ethernet PHY not found - u-boot migration

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,821 Views
charleshuang
Senior Contributor II

Hi Igor,

It is working when I change PHYADDR from 1 to 4, thanks.

0 Kudos