U-Boot Does not work with i.MX6Q and MMPF0100 default F0 ROM.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-Boot Does not work with i.MX6Q and MMPF0100 default F0 ROM.

884 Views
takashitakahash
Contributor III

Dear community.

Our customer has question below.

Customer evaluating own board using CPU: i.MX6Quad, PMIC: MMPF0100F0ANESR2.

 But when power supply  problems occur that boot from the boot device (eMMC used) specified by the BOOT_CFG pin of the CPU .

By the way, it will start up by manually controlling the reset signal POR_B (H → L → H)is no problem, we believe there is no mistake in the setting of the BOOT_CFG pin itself.

For the cause investigation, the power supply start sequence of SABRE - SDB and customer board was compared.

As a problem, on the customer board, it turned out that POR_B output by PMIC was controlled to H (reset release) before VDDARM_CAP was output.

※ In the SABRE-SDB, this order is reverse.

This is contrary to the following description of the reference manual IMX6DQRM, P.5084, so I think that a problem has occurred.

60.5.1 External POR using SRC_POR_B

If the external SRC_POR_B signal is used to control the processor POR, SRC_POR_B must remain low (asserted) until the VDD_ARM_CAP and VDD_SOC_CAP supplies are stable.

<question>

1, Does SABRE - SDB use the default "F 0 "OTP setting?

    Customer used F0 OTP settings.

2,Is SABRE-SDB doing OTP rewriting / customization from the default "F0"?

3,On the SABRE-SDB, when "F0" OTP is being rewritten, which address
   What kind of values are  rewriting?

4,When OTP is not rewritten, what will be assumed as the reason for the difference in the timing of the power supply     

   startup sequence between the SABRE-SDB and customer board?

5,I tried AN4546 (MMPF0100 OTP Programming Instructions) method to change the PMIC timing, but I could read  

   registers other than OTP, but I can not access the OTP region register.
   Address 0x80 Is OTP FUSE READ EN required to write 0x01 before reading OTP?

6,When the output voltage of MCIMX 6Q-SDB was measured with an oscilloscope here
In the default sequence of PMIC F 0
   9th VGEN 1
   10th VGEN 2
   11th VGEN 3
   12 th VGEN 5,
  
In actual measurement
VGEN 1 and VGEN 2, VGEN 3 and VGEN 5 are running at the same timing, respectively.
Is it a custom OTP rather than the default sequence of F0?

Thank you,

Best Regards.

T.Takahashi.

Labels (3)
0 Kudos
1 Reply

668 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Takahashi,

  

1, Does SABRE - SDB use the default "F 0 "OTP setting?

    Customer used F0 OTP settings.

Yes,it does. F0 is correct.

2,Is SABRE-SDB doing OTP rewriting / customization from the default "F0"?

No, it is not. if OTP was done, it can't be done again.

3,On the SABRE-SDB, when "F0" OTP is being rewritten, which address
   What kind of values are  rewriting?

About F0, We have a script provided by Power team, you should download it from offical website.

But MMPF0100F0ANES is F0 configuration, customer can't do OTP again.

4,When OTP is not rewritten, what will be assumed as the reason for the difference in the timing of the power supply     

   startup sequence between the SABRE-SDB and customer board?

you can check follwing items when power up:

(1) Is PWRON pin HIGH?

(2) Is VDDOTP pin is LOW?( the status is "start up from OTP)"?

(3) Does VSNVS output 3.0V?

(4) Is POR_B pin of CPU HIGH?

5,I tried AN4546 (MMPF0100 OTP Programming Instructions) method to change the PMIC timing, but I could read  

   registers other than OTP, but I can not access the OTP region register.
   Address 0x80 Is OTP FUSE READ EN required to write 0x01 before reading OTP?

pastedImage_2.png

0x7F register should be 0x01 / 0x02. then you can read OTP registers.

6,When the output voltage of MCIMX 6Q-SDB was measured with an oscilloscope here
In the default sequence of PMIC F 0
   9th VGEN 1
   10th VGEN 2
   11th VGEN 3
   12 th VGEN 5,

these VGENs can't affect CPU booting.

>>Is it a custom OTP rather than the default sequence of F0?

It is the default sequence of F0.

Best Regards,

Weidong

0 Kudos