Two non-overlapping windows or Picture-in-picture

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Two non-overlapping windows or Picture-in-picture

361 Views
zillian
Contributor I

Hi !

 There are descrptions "Two non-overlapping windows" "Picture-in-picture "In IMX6DQRM.pdf page 459 about it's supported applications.  I  have added two camera devices and corresponding drivers in SABRESD board. Each camera can work in test-pattern mode and can display chess board on LCD in OVERLAY way. But I am not able to display two camera images on one LCD simultaneous. could anybody give some clues ?

Labels (1)
0 Kudos
1 Reply

296 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi tang,

You may try using overlaysink plugin, as described in section 7.5 (Overlaysink usage) of

“i.MX_Linux_User's_Guide.pdf” :

 

“The overlaysink plugin is based on the GPU. It provides two main functions for video rendering:

• Video Overlay: composites multiple video playbacks into the same display.

• Multiple Display: shows videos to multiple displays, up to four displays.”

 

Please refer to section 7.3.1.6.3 (Multiple videos overlay) for example.

 

Also, please look at section 7.3.16 (Video composition).

https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fwebapp%2FDownload%3FcolC... 

Regards

0 Kudos