Two frame in one screen..(IMX6,SABRE Lite,Aptina sensor)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Two frame in one screen..(IMX6,SABRE Lite,Aptina sensor)

910 Views
elliottyang
Contributor II

Hi ALL

I have finished the Linux driver for CMOS sensor (Aptina AP0100+AR0130).

When I used gstreamer to see the image, I saw two frame in one screen, shows below:

相片 2014-6-25 16 52 29.jpg

Here is my command of gstreamer:  gst-launch-0.10 mfw_v4lsrc capture-mode=0 ! mfw_v4lsink

This is a Yocoto project, the kernel version is 3.10.17.

My demo board is SABRE Lite.

Does anyone can help me ? thanks a lot..

Elliott

0 Kudos
1 Reply

363 Views
amadeusholmer
Contributor I

Hello Elliott,

I think its a long time from your post but I hope you are still active and that you can help me. I also want to get the AR0130 sensor running on an iMX6 board (Variscite Dart-MX6) with Yocto. I do not have a driver and now I found your post where your wrote you have one finished.

Do you have a driver for the AR0130 that you can provide to me (and the community respectively)?

Thanks for any effort.

Bests

Amadeus

0 Kudos