Two displays support via HDMI and MIPI-DSI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Two displays support via HDMI and MIPI-DSI

跳至解决方案
3,724 次查看
dmitrykonyshev
Contributor II

Hello,

Is it possible to use HDMI and MIPI-DSI at the same time to create a two-display system? It doesn't seem to be explicitly stated in the documentation. In the sample EVK device trees with MIPI-DSI (fsl-imx8mq-evk-lcdif-rm67191.dts and fsl-imx8mq-evk-lcdif-adv7535.dts) the HDMI is disabled. Is it because it's impossible to use both in parallel or there's another reason for this?

Regards,

Dmitry

标记 (2)
0 项奖励
回复
1 解答
2,959 次查看
felixradensky
Contributor IV

Hi Dmitry,

The relevant DTS file is fsl-imx8mq-evk-dual-display.dts. The following article may be helpful: How to use dual display on i.MX8 including 4k decoding - i.MXDev Blog 

Felix.

在原帖中查看解决方案

2 回复数
2,960 次查看
felixradensky
Contributor IV

Hi Dmitry,

The relevant DTS file is fsl-imx8mq-evk-dual-display.dts. The following article may be helpful: How to use dual display on i.MX8 including 4k decoding - i.MXDev Blog 

Felix.

2,959 次查看
dmitrykonyshev
Contributor II

Thank you, Felix!

0 项奖励
回复