Two displays support via HDMI and MIPI-DSI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Two displays support via HDMI and MIPI-DSI

ソリューションへジャンプ
1,867件の閲覧回数
dmitrykonyshev
Contributor II

Hello,

Is it possible to use HDMI and MIPI-DSI at the same time to create a two-display system? It doesn't seem to be explicitly stated in the documentation. In the sample EVK device trees with MIPI-DSI (fsl-imx8mq-evk-lcdif-rm67191.dts and fsl-imx8mq-evk-lcdif-adv7535.dts) the HDMI is disabled. Is it because it's impossible to use both in parallel or there's another reason for this?

Regards,

Dmitry

タグ(2)
0 件の賞賛
1 解決策
1,102件の閲覧回数
felixradensky
Contributor IV

Hi Dmitry,

The relevant DTS file is fsl-imx8mq-evk-dual-display.dts. The following article may be helpful: How to use dual display on i.MX8 including 4k decoding - i.MXDev Blog 

Felix.

元の投稿で解決策を見る

2 返答(返信)
1,103件の閲覧回数
felixradensky
Contributor IV

Hi Dmitry,

The relevant DTS file is fsl-imx8mq-evk-dual-display.dts. The following article may be helpful: How to use dual display on i.MX8 including 4k decoding - i.MXDev Blog 

Felix.

1,102件の閲覧回数
dmitrykonyshev
Contributor II

Thank you, Felix!

0 件の賞賛