Two displays support via HDMI and MIPI-DSI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Two displays support via HDMI and MIPI-DSI

Jump to solution
3,894 Views
dmitrykonyshev
Contributor II

Hello,

Is it possible to use HDMI and MIPI-DSI at the same time to create a two-display system? It doesn't seem to be explicitly stated in the documentation. In the sample EVK device trees with MIPI-DSI (fsl-imx8mq-evk-lcdif-rm67191.dts and fsl-imx8mq-evk-lcdif-adv7535.dts) the HDMI is disabled. Is it because it's impossible to use both in parallel or there's another reason for this?

Regards,

Dmitry

Tags (2)
0 Kudos
Reply
1 Solution
3,129 Views
felixradensky
Contributor IV

Hi Dmitry,

The relevant DTS file is fsl-imx8mq-evk-dual-display.dts. The following article may be helpful: How to use dual display on i.MX8 including 4k decoding - i.MXDev Blog 

Felix.

View solution in original post

2 Replies
3,130 Views
felixradensky
Contributor IV

Hi Dmitry,

The relevant DTS file is fsl-imx8mq-evk-dual-display.dts. The following article may be helpful: How to use dual display on i.MX8 including 4k decoding - i.MXDev Blog 

Felix.

3,129 Views
dmitrykonyshev
Contributor II

Thank you, Felix!

0 Kudos
Reply