Hi all,
we want to connect two external PHY (LAN8720A) on i.MX6 Solo (RMII interface).
Refer to
i.MX 6SoloX Applications Processor Reference Manual, Rev. 0, 2/2015
24.3 External Signals, the table describes the external signals of ENET1 and ENET2.
I match the ENET1 signals:
ENET1_MDC = RMII_MDC
ENET1_MDIO = RMII_MDIO
ENET1_RX_DATA0 = RMII_RX_DATA0
ENET1_RX_DATA1 = RMII_RX_DATA1
ENET1_TX_DATA0 = RMII_TX_DATA0
ENET1_TX_DATA1 = RMII_TX_DATA1
ENET1_RX_ER = RMII_RX_ER
ENET1_RX_EN = RMII_CRS_DV
ENET1_REF_CLK1 = RMII_25MHz_PHY_CLK
Is that correct?
Is the signal ENET1_REF_CLK1 in the right power domain?
Could I use the ENET1_REF_CLK1 to clock the PHY?
I found in the table a signal "ENET1_REF_CLK_25MHz",
but there is no Mode given (" - ").
Could you please let me know - what does it mean?
Regards
Erich
解決済! 解決策の投稿を見る。
Hello Erich,
See following, please !
-----PHY Clock : ENET2_RX_CLK pin can be multiplexed as ENET_REF_CLK_25M, which is for PHY Clock.
The level is determined by the voltage of NVCC_ENET, on evk board, the level is 3.3V. you should check the phy's datasheet you are using, then decide if level shifter will be used.
that is : ENET2_RX_CLK pin --->ENET_REF_CLK_25M(3.3V)--->level shifter(if needed)--->PHY's clock input pin(XTLI)
Hope above suggestion can help you !
Regards,
Weidong
Hello Weidong,
thanks a lot, I will use ENET2_RX_CLK.
Regards
Erich
Hello Erich,
See following, please !
-----PHY Clock : ENET2_RX_CLK pin can be multiplexed as ENET_REF_CLK_25M, which is for PHY Clock.
The level is determined by the voltage of NVCC_ENET, on evk board, the level is 3.3V. you should check the phy's datasheet you are using, then decide if level shifter will be used.
that is : ENET2_RX_CLK pin --->ENET_REF_CLK_25M(3.3V)--->level shifter(if needed)--->PHY's clock input pin(XTLI)
Hope above suggestion can help you !
Regards,
Weidong