Two LVDS with overlays on mx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Two LVDS with overlays on mx6

1,700 Views
andreapicaro
Contributor I

Hello, on our imx6 quad based board we are tryng to configure two LVDS displays.

I can correctly bring them on through board file configurations:

static struct ipuv3_fb_platform_data fb_data[] =

        {

            {

               .disp_dev = "ldb",

               .interface_pix_fmt = IPU_PIX_FMT_RGB666,

               .mode_str = "1024600",

               .default_bpp = 16,

               .int_clk = false,

               .late_init = false,

            },

            {

               .disp_dev = "ldb",

               .interface_pix_fmt = IPU_PIX_FMT_RGB24,

               .mode_str = "800480",

               .default_bpp = 16,

               .int_clk = false,

               .late_init = false,

            },

}

and

static struct fsl_mxc_ldb_platform_data ldb_data = { .ipu_id = 0, .disp_id = 0,

            .ext_ref = 1, .mode = LDB_SEP1, .sec_ipu_id = 1, .sec_disp_id = 1, };

My problem is that displays are always set up as fb0 + fb1 and fb2 but i'd like to have overlay on both channels;

from my understanding of ipu I should configure first display as ipu0 - display0  and second as ipu1 - display0 thus obtaininig

fb0 + fb1 and fb3 + fb4. I tried many solutions but nothing seems to work. I suppose i'm missing something.

Can you give me any hint or point me to some documentation explaining in detail mx6 frame buffers configurations?

Thank you!

Labels (2)
0 Kudos
Reply
1 Reply

1,234 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andrea

for old kernel there is quite good description on

Linux Software User Manual (i.MX6) - BlueWiki

https://www.kernel.org/doc/Documentation/fb/framebuffer.txt

for last kernel, seems one needs to look at sources (mxc_ipuv3_fb.c),

attached Linux Manual also may be helpful.

Best regards

igor

0 Kudos
Reply