Hi there,
I've been trying to get the SPI periphal running with Zephyr on the RT1020 evaluation board. Sadly,
I get a very unspecific error:
undefined reference to `__device_dts_ord_83'
My prj.conf looks like this:
CONFIG_GPIO=y
CONFIG_SPI=y
I tried other arguments like CONFIG_SPI_ASYNC but that did not change anything.
I am using an .overlay file to add an SPI device:
&lpspi1 {
trinamic: trinamic@0 {
compatible = "vnd,spi-device";
reg = <0>;
spi-max-frequency = <100000>;
label = "trinamic";
};
};
My code looks like that:
Spoiler#include <zephyr.h>
#include <drivers/spi.h>
#include <drivers/gpio.h>
#define SPI_TEST_DEV DT_COMPAT_GET_ANY_STATUS_OKAY(trinamic)
#define SPI_OP SPI_OP_MODE_MASTER | SPI_MODE_CPOL | SPI_MODE_CPHA | SPI_WORD_SET(8) | SPI_LINES_SINGLE
uint8_t my_buffer[4] = {1, 1, 1, 1};
struct spi_buf my_spi_buffer[1];
const struct spi_buf_set tx_buff = {my_spi_buffer, 1};
const struct spi_dt_spec spi_dev =
SPI_DT_SPEC_GET(DT_NODELABEL(trinamic), SPI_OP, 0);
uint8_t once = 0;
void main(void)
{
if (once == 0)
{
my_spi_buffer[0].buf = my_buffer;
my_spi_buffer[0].len = 4;
spi_write_dt(&spi_dev, &tx_buff);
once = 1;
}
}
I don't really get it, sadly the loopback spi example is quite confusing aswell. It would be very kind if someone could help me! Thank you very much.
All the best