Trying to run mir desktop on imx6dl

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trying to run mir desktop on imx6dl

1,756件の閲覧回数
tarakpatel
Contributor I

Hi,

I have custom imx6dl-sabresd board. I have ubuntu 16.04 desktop installed on it and tried to run miral-app and i got following errors.

gbm: driver exports no extensions (/usr/lib/arm-linux-gnueabihf/dri/vivante_dri.so: undefined symbol: __driDriverExtensions)failed to load driver: vivante

May i know from where i can get source code to compile vivante_dri.so? or how to get rid of this error from the specified driver? 

Thanks,

Tarak Patel

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

1,627件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tarak

vivante_dri.so is described Table 13-2. GPU Library Files attached Linux Manual,

in NXP BSPs seems it is provided in binary only as mentioned on p.109 document:

"The GPU driver kernel module source is in the kernel source tree, but the libs are
delivered as binary only."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,627件の閲覧回数
tarakpatel
Contributor I

Hi Igor,

Thanks for your reply. Have you seen any instance of above error, or anyone porting ubuntu core on imx6dl sabresd board. The problem is this os only supports mir-kiosk(i.e. miral) and wayland as a GUI platforms and both of them uses DRM backend. Whenever i run using DRM backend i will get above error. Is their a way to work around or do freescale have vivante_dri.so binary which has above mentioned symbol in it.

Please also correct my understanding if i have mentioned something wrong.

Thanks for your time and help.

Thanks,

Tarak Patel

0 件の賞賛
返信

1,627件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tarak

one can try with boundary devices ubuntu

Ubuntu - Boundary Devices 


Best regards
igor

0 件の賞賛
返信