Trying to boot different OSes on A53 and M7 cores of my i.Mx8 Nano Evaluation board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trying to boot different OSes on A53 and M7 cores of my i.Mx8 Nano Evaluation board.

701 Views
anurag16doshi
Contributor II

I am looking to boot up the Cortex A53 with one OS and the Cortex M7 with another. I am looking to be able to boot the OSes independently. I want them to run on their own without having to dependent on the other for booting up capabilities. I also do not want to use one of the OSes to start boot process of the other as well. If there is a document that any one can direct me to or help me to achieve this I would highly appreciate it.

Thanks,

Anurag

imx8mnevk multicore‌ mbed os‌a53#cortex m7

Labels (1)
0 Kudos
1 Reply

669 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Anurag,

You can refer to "Running the Arm Cortex-M4 image" of Linux User's Guide for running the M4 image. in the MX8Nano.

Regards

0 Kudos