Try L2.6.35_11.09.01_ER_source on i.MX35 3Stack board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Try L2.6.35_11.09.01_ER_source on i.MX35 3Stack board

953 Views
VincentChou1z
Contributor III

Hi!  I would like to ask whether anyone has experience to build the image for i.MX35 3 Stack board based on L2.6.35_11.09.01_ER_source.  I found the option exists in LTIB but I could not boot the board with the u-boot, kernel and rootfs based on the source.  Any suggestion?

0 Kudos
Reply
2 Replies

818 Views
VincentChou1z
Contributor III

I managed to boot i.MX35 3stack PDK with U-Boot on SD Card and it did go pass the boot stage and hanged at the same place like you came across: Uncompress Linux.  I used 2.6.35 09 source code provided by freescale.  I guess the problem is from the source code itself.  However, I did some research and discovered some people do run 2.6.35 on i.MX35 3Stack board.  How did they do that?

0 Kudos
Reply

818 Views
MartenLootsma1z
Contributor I
One year ago we tried to boot an image of the 2.6.35,without success as well. The difference innour setup is that our bootloader is redboot, but that does not seem to make differences.
0 Kudos
Reply