Trusty TEE support in iMX8 Mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trusty TEE support in iMX8 Mini

3,378 Views
msingh1920
Contributor V

Hi Sir,

I am planning to use iMX 8 Mini for my project.
On security and Trusted Execution Environment (TEE) pdf document of NXP it is mentioned that iMX8 Mini comes with Trusted Execution Environment (TEE).
and In Android, Trusty is a secure Operating System (OS) that provides a Trusted Execution Environment (TEE).
so I want to know that -

1. Is Trusty included in Android package provided by NXP for iMX 8 Mini?
2. Can you please provide more information about how to get and use Trusty TEE for iMX 8 ?

Thanks & Regards,
Maneesh Singh

5 Replies

2,601 Views
haoranwang
NXP Employee
NXP Employee

Hi maneeshsingh‌,

    You can evaluate Trusty OS on imx8M Mini by below modification in evk_8mm.mk:

PRODUCT_IMX_TRUSTY := true

     Thanks.

0 Kudos
Reply

2,600 Views
jaganteki
Contributor I

Thanks for the point haoranwang‌ can you link the desired repo, I would like to build and verify TEE Android on i.MX8M mini.

0 Kudos
Reply

2,601 Views
abhijit_thorat
Contributor III

Hi Maneesh,

I know TEE OS from OP-TEE is supported but not sure about Trusty TEE OS.

Any NXP member can confirm this and have any information about this?

0 Kudos
Reply

2,600 Views
baodongchen
Contributor II
0 Kudos
Reply

2,601 Views
msingh1920
Contributor V

Hi ,

Is anyone from NXP can reply to my above question ? 
I just want to know - 

1. Is Trusty TEE OS supplied by Android is supported on iMX8 mini platform or not ?
2. If it is supported then how to port it on iMX 8 mini ?

please help me to solve this issue.

Thanks & Regards,
Maneesh Singh

0 Kudos
Reply