[Troubles]Ltib compilation with the profile FSL gnome release packages

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Troubles]Ltib compilation with the profile FSL gnome release packages

4,790 Views
Florentino
Contributor I

Hi everybody,


I’m trying to compile a Linux distribution for an i.mx6 board with Gnome but I have some troubles!
Firstly, you need to know that I work with: L3.0.15_12.04.01_ER_source.tar.gz
And my compilation with the minimal profile was a success (without X).
Now I want to try my build a HMI, but my compilation failed when I arrived on the Gnome-vst package, I have this error message (the commands are in bold, the results italic )


./ltib --preconfig config/platform/imx/imx6q.cf --profile config/platform/imx/release_gnome.profile
/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find -lgssapi_krb5
/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find -lkrb5
/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find -lk5crypto
collect2: ld returned 1 exit status
make[2]: *** [libftp.la] Error 1
make[2]: Leaving directory `/home/psa/Ltib/ltib/rpm/BUILD/gnome-vfs-2.24.1/modules'
make[1]: *** [all-recursive] Error 1
make[1]: Leaving directory `/home/psa/Ltib/ltib/rpm/BUILD/gnome-vfs-2.24.1'
make: *** [all] Error 2
error: Bad exit status from /home/psa/Ltib/ltib/tmp/rpm-tmp.46078 (%build)

RPM build errors:
    Bad exit status from /home/psa/Ltib/ltib/tmp/rpm-tmp.46078 (%build)
Build time for gnome-vfs: 23 seconds
Failed building gnome-vfs

So I tried to compile the Kerberos package alone. There was no krb5-1.3.4.tar.gz in my sources, but there were the patch krb5-fix-build-error.patch and the spec file kbr5.spec.


You can watch two files in attached files.


The kbr5.spec do reference at two others patches:
Patch1          : kbr5-1.3.4-fix-EAI_NODATA-undefined-check.patch
Patch2          : kbr5-1.3.4-fix-conflicting-types-for-getline.patch


I could download kb5.1.3.tar.gz. But, I could'nt find these patches on web.
I have tried to compile kb5-1.3.4.tar.gz without the two patches (I have commented the lines ,where there were references  to thes patches) ,and I have thes messages..:

./ltib -m prep krb5.spec -p krb5
+ echo Patch #0 (krb5-fix-build-error.patch):
Patch #0 (krb5-fix-build-error.patch):
+ patch -p1 -s
+ exit 0
Build time for krb5: 1 seconds


And :


./ltib -m scbuild krb5.spec -p krb5
cd krb5-1.3.4
+ ac_cv_func_regcomp=yes ac_cv_file__etc_environment=yes ac_cv_file__etc_TIMEZONE=yes ac_cv_func_res_search=yes
/home/psa/Ltib/ltib/tmp/rpm-tmp.41503: 1: ac_cv_func_regcomp=yes ac_cv_file__etc_environment=yes ac_cv_file__etc_TIMEZONE=yes ac_cv_func_res_search=yes: not found
error: Bad exit status from /home/psa/Ltib/ltib/tmp/rpm-tmp.41503 (%build)
RPM build errors:
    Bad exit status from /home/psa/Ltib/ltib/tmp/rpm-tmp.41503 (%build)
Build time for krb5: 0 seconds
Failed building krb5
f_scbuild() returned an error, exiting


So, maybe somebody have the same problem or could help me.
I have hope in the i.MX community :)
Thanks
Best regards


Florent

Original Attachment has been moved to: 30-krb5fixbuilderror.patch

Original Attachment has been moved to: 29-krb5.spec

Labels (1)
Tags (2)
0 Kudos
Reply
5 Replies

2,371 Views
praveeng
Contributor II

Can you please tell me , from which link  did you download the LTIB for iMX6. I am also in need of L3.0.15_12.04.01_ER_source.tar.gz

0 Kudos
Reply

2,371 Views
hpdwally
Contributor II

I think these may have been taken down?

0 Kudos
Reply

2,371 Views
jimmychan
NXP TechSupport
NXP TechSupport


For the "cannot find -lgssapi_krb5" problem , just simply to remove or rename the /usr/bin/krb5-config file.

0 Kudos
Reply

2,371 Views
Florentino
Contributor I

Yep of course, that's what I did and that was what I have forgot to tell here

"So I tried to compile the Kerberos package alone. There was no krb5-1.3.4.tar.gz in my sources, but there were the patch krb5-fix-build-error.patch and the spec file kbr5.spec."

Thank you even :)

H R Krishna Pavan said:

Hi,


Find krb5-1.3.4.tar.gz and place it in your packages directory.

The same applies to the other missing softwares also.

You may have to do this for many other packages, if they are not present, but required by you! It works.

0 Kudos
Reply

2,371 Views
KrishnaPavan
Contributor II

Hi,


Find krb5-1.3.4.tar.gz and place it in your packages directory.

The same applies to the other missing softwares also.

You may have to do this for many other packages, if they are not present, but required by you! It works.

0 Kudos
Reply