Hi
I am new to embedded system.
I am using i.mx6dl on a custom board running ubuntu 16.04.
Linux kernel: 4.1.15
I have to integrate murata wifi module using sdio interface for which the gpio pin number 33 and 116 has to be low during bootup.
I have tried the make them low in the following manner
I checked the status of gpios. I can see 33 and 116 are set to low
But after rebooting it and again I checked the status. Those pins are not present.
I checked those pins using multimeter, they are still high.
How can I make them low during boot up.
Thanks
Hi alam1
pins state is not retained after rebooting, it is set to values described in
Table 97. 21 x 21 mm Functional Contact Assignments, column "Out of Reset Condition"
i.MX 6Solo/6DualLite Applications Processors for Consumer Products
Best regards
igor
Hi igor
I checked the table which you have mentioned.
The pins are set to high.
How can I make them low?
I tried to make low from uboot, still the problem is not solved.
>How can I make them low?
there is no way to change it after reset, as it is defined in hardware.
One can set necessary value for example in uboot/
Best regards
igor
I made them low from uboot.
But the issue is its still high after reboot.
I checked it with multimeter.
I want to the pins to low during bootup and then get high.
Is this possible??
Thanks
no this is not possible as it is defined in hardware.
Best regards
igor