Transient response of Power line

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Transient response of Power line

1,407 次查看
ban45
Contributor III

Is there a standard for the transient response of the power line (i.e. NVCC_DRAM) of i.MX6?
Shouldn't the input voltage range be exceeded?
Could you tell me where to put the data sheet?

I think power response is a problem,
but Is there anything that can be done on the CPU side?

标签 (3)
0 项奖励
回复
3 回复数

1,314 次查看
igorpadykov
NXP Employee
NXP Employee

Hi  Yasunori

for NVCC_DRAM  of i.MX6S power supply requirements one can follow
Table 8. Operating Ranges, sect.4.2.1 Power-Up Sequence i.MX6S Datasheet
https://www.nxp.com/docs/en/data-sheet/IMX6SDLCEC.pdf 
and ripples requirements defined in Table 2-6. Power and decouple recommendations
i.MX6DQSDL Hardware Guide:
https://www.nxp.com/webapp/Download?colCode=IMX6DQ6SDLHDG

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,314 次查看
ban45
Contributor III

Thank you igorpadykov.

i.MX6DQSDL Hardware Guide.

The following contents were described in the guide.

"Common requirement for ripple noise should be less
than 5% Vp-p of supply voltage average value.
Related power rails affected: all VDD_xxx_IN and
VDD_xxx_CAP."

Is it safe to operate even if 5% Vp-p exceeds the input range?

0 项奖励
回复

1,314 次查看
igorpadykov
NXP Employee
NXP Employee

>Is it safe to operate even if 5% Vp-p exceeds the input range?

sorry, values in Table 8. Operating Ranges should not be exceeded.

Best regards
igor

0 项奖励
回复