Transformer networks on i.MX 8M Plus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Transformer networks on i.MX 8M Plus

2,375 Views
GeraldK
Contributor II

Hello everyone,

NXP presented the i.MX 95 earlier this year and with it the new eIQ Neutron NPU. As mentioned on their page it supports transformer network architectures. So I am wondering, if this only holds to the neutron NPU. Or are transformers also possible on the NPU of the 8M+? Does anyone have knowldege about that?

IMX8MPLUS

Tags (1)
0 Kudos
Reply
5 Replies

2,218 Views
RizHsu
Contributor I

I'm also interested in this. May I know if it's possible to run a transformer model on the i.MX 8M Plus?

Since we currently cannot purchase a i.MX95 EVK without joining the early access plan, so we would like to use the i.MX 8M for doing early evaluation on our ML solution.

0 Kudos
Reply

2,336 Views
joanxie
NXP TechSupport
NXP TechSupport

let me confirm it and tell you later

0 Kudos
Reply

2,146 Views
jlamp
Contributor II
Hi @joanxie I am also interested in running transformer models in the i.MX 8M Plus. Do you have any information?

Regards,
0 Kudos
Reply

2,133 Views
joanxie
NXP TechSupport
NXP TechSupport

Transformer networks are supported, however, the performance really depends upon the model architecture.

0 Kudos
Reply

2,113 Views
jlamp
Contributor II

Hi @joanxie can you tell me which transformer models are supported?

I am trying the Visual Transformers (ViT) and I am not able run them using NPU...

Regards!

0 Kudos
Reply