Transformer networks on i.MX 8M Plus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Transformer networks on i.MX 8M Plus

2,290件の閲覧回数
GeraldK
Contributor II

Hello everyone,

NXP presented the i.MX 95 earlier this year and with it the new eIQ Neutron NPU. As mentioned on their page it supports transformer network architectures. So I am wondering, if this only holds to the neutron NPU. Or are transformers also possible on the NPU of the 8M+? Does anyone have knowldege about that?

IMX8MPLUS

ラベル(1)
タグ(1)
0 件の賞賛
返信
5 返答(返信)

2,133件の閲覧回数
RizHsu
Contributor I

I'm also interested in this. May I know if it's possible to run a transformer model on the i.MX 8M Plus?

Since we currently cannot purchase a i.MX95 EVK without joining the early access plan, so we would like to use the i.MX 8M for doing early evaluation on our ML solution.

0 件の賞賛
返信

2,251件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

let me confirm it and tell you later

0 件の賞賛
返信

2,061件の閲覧回数
jlamp
Contributor II
Hi @joanxie I am also interested in running transformer models in the i.MX 8M Plus. Do you have any information?

Regards,
0 件の賞賛
返信

2,048件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

Transformer networks are supported, however, the performance really depends upon the model architecture.

0 件の賞賛
返信

2,028件の閲覧回数
jlamp
Contributor II

Hi @joanxie can you tell me which transformer models are supported?

I am trying the Visual Transformers (ViT) and I am not able run them using NPU...

Regards!

0 件の賞賛
返信