Transfer SGTL5000 data to iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Transfer SGTL5000 data to iMX6

795 Views
purvi_billore1
Contributor III

I am working to design a full duplex telephonic system and I want to send and receive audio data in real time. Therefore,

I have preferred this link https://community.nxp.com/thread/490784.

Can I have sample code to use circular buffer instead of file while transferring the audio data from SGTL5000 audio codec connected to iMX6 over EIM bus.

(example: for telephonic system )

sgtl500‌ imx linux imx6 

Thanks and Regards,

Purvi

Labels (3)
2 Replies

670 Views
igorpadykov
NXP Employee
NXP Employee

Hi Purvi

unfortunately I am not aware of such sample codes, in general nxp has special

service for helping with software developing and customizations:

NXP Professional Services | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

670 Views
abhijeet_ghodga
Contributor III

Hi Igor,

Ping-pong buffer C code has been implemented till now and the data is sent over the EIM bus. But there is no way to check if it is real-time or the loopback is happening correctly.

I am happy to share the modifications done on the aplay c file.

Best,

Abhijeet

0 Kudos
Reply