Hi ,
We are porting android kitkat to SAMA5D3 development board which is of size 480*272 (pixel), only partial touch input is happening like drop down and Setting page when I keep giving inputs randomly and nothing else. But touch works well with Evaluation Kit which is of size 800*600 (pixel length).
The cause of touch issue is, it is taking requested height as 19 instead of 480 in WindowManagerService. Please refer the below log.
I/WindowManagerService( 1418): relayoutWindow  win.mRequestedWidth272
I/WindowManagerService( 1418): relayoutWindow  win.mRequestedHeight19
I/WindowManagerService( 1418): AOSP:::updateFocusedWindowLocked
I/WindowManagerService( 1418): AOSP:::computeFocusedWindowLocked
Original Attachment has been moved to: logs.zip
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi archana
one can try Calibrate.APK as described for example on
How-To: Fix Touchscreen Issues in Android Phones
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------