Toolchain for i.mx28

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Toolchain for i.mx28

1,279件の閲覧回数
tomhanks
Contributor I

I am trying to get a build going for i.mx28.  I've downreved Ubuntu to 10.10 which allows me to install LTIB, which seems to be required, but I can't get a g++ install for the old version of Ubuntu.  If I use a more recent version of Ubuntu, I can't get LTIB installed.

What's the current toolchain setup I should be using for a linux application for i.mx28?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,038件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tom

for new ubuntu one can look at suggestions provided on

imx6q build LTIB problems 

or use some third party yocto releases, like:

http://www.digi.com/support/productdetail?pid=5587&type=documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信