Tool to compile IM6 source code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Tool to compile IM6 source code

1,555 次查看
lyfsci
Contributor III

Hi Experts,


Is there any installation or tool required to compile the linux source code of the IMX6 SL processor. for EVK ?

I had downloaded the IMX6 source code and was looking for tool to compile it.

标签 (1)
0 项奖励
回复
2 回复数

1,463 次查看
lyfsci
Contributor III

Thats great info.

0 项奖励
回复

1,463 次查看
Yuri
NXP Employee
NXP Employee

   It may be recommended to use the recent Linux BSP(s) for i.MX6 (SL ).

https://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.2_iMX6SL_BUNDLE&appType=license&locat...

https://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.0_IMX6SL_BUNDLE&appType=license&locat...

http://cache.freescale.com/files/32bit/doc/support_info/IMX6YOCTOPATCHRN.pdf

https://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.0_LINUX_DOCS&appType=license&location...

The documentation package (L3.10.17_1.0.0_LINUX_DOCS) / file (IMX6YOCTOPATCHRN.pdf)

contains information how to setup host environment and build target system.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复