Toggle GPIO pins of IMX8MM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Toggle GPIO pins of IMX8MM

1,712件の閲覧回数
divyeshmarne0
Contributor III

Hi Team,

Need your inputs here.

I want to toggle few PINS of IMX8mm based on signal and operations.

Like sometimes i have to mute the Amplifier. for that I have pull HIGH gpio3_IO24. LED to turn ON /OFF for sometimes. How to play with GPIO . which driver we can use in NXP code base Android 11.

Can you provide inputs here, how we can toggle these pins and In which driver we can do that.

Please provide example if possible.

SD_GPIO (SHUTDOWN)SAI5_RXD0GPIO3_IO21
Fault_GPIOSAI5_RXFSGPIO3_IO19
PLIMITSAI5_RXD2GPIO3_IO23
MUTE_GPIOSAI5_RXD3GPIO3_IO24
CODEC_20W_RESETSAI3_RXFSGPIO4_IO28
CODEC_0.8W_RESETSAI1_RXCGPIO4_IO1
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,694件の閲覧回数
divyeshmarne0
Contributor III

Hi Team,

Please update on above case.

0 件の賞賛
返信

1,668件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信