To effect secure boot immediately, which boot sequence does it need?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

To effect secure boot immediately, which boot sequence does it need?

跳至解决方案
4,640 次查看
takayuki_ishii
Contributor V

Hello community

In Document "i.MX_6_Linux_High_Assurance_Boot_(HAB)_Users_Guide_201405.pdf",

It have a sequence to put SEC_CONFIG to close in section 4 "Test Procedure".

After write eFuse by echo command,

In chapter 19, it say that "Boot the board again,",

Is this mean that to effect the chip security immediately, it must need a power on/off cycle?

Or it need only reset (POR_B Low cycle) to do that?

To reduce the eFuse write cycle time, customer plan to use "POR_B" cycle for it.

Best regards,

Ishii.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,036 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

you are right, to effect the chip security immediately it is

sufficient only reset (POR_B Low cycle) to do that.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,036 次查看
takayuki_ishii
Contributor V

Hello Igor,

Thank you for your quick response.

I will answer it to my customer.

Best regards,

Ishii.

0 项奖励
回复
1,037 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

you are right, to effect the chip security immediately it is

sufficient only reset (POR_B Low cycle) to do that.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复