To Wigros Sun, 在iMX6DQ上使用USB TO ETHERNET 芯片同时扩展2个网络口可以吗

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

To Wigros Sun, 在iMX6DQ上使用USB TO ETHERNET 芯片同时扩展2个网络口可以吗

Jump to solution
711 Views
shine_wang
Contributor I

我们想在iMX6DQ的板子上,USB HOST1 上先用USB-HUB芯片扩展出4个USB口,再用2个USB TO ETHERNET芯片扩展两个网络口,这样可以吗,速度上会有影响吗

Labels (2)
0 Kudos
1 Solution
595 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Shenghua,

   We have several way to expand ethernet interface:

1. USB port

Just as what you said, USB HOST-->usb hub with 4 ports--> two of 4 ports--> USB to ethernet bridge)-->2 ethernet ports

the way is no problem, if you want speed 10/100Mbps, it is no problem.

2. PCIe port

You can use intel82574 or intel82574it(industrial grade) and connect it to PCIe port.

Above both methods are feasible.

Hope above advice is helpful for you.

Have a nice day!

BR,

Weidong

View solution in original post

0 Kudos
1 Reply
596 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Shenghua,

   We have several way to expand ethernet interface:

1. USB port

Just as what you said, USB HOST-->usb hub with 4 ports--> two of 4 ports--> USB to ethernet bridge)-->2 ethernet ports

the way is no problem, if you want speed 10/100Mbps, it is no problem.

2. PCIe port

You can use intel82574 or intel82574it(industrial grade) and connect it to PCIe port.

Above both methods are feasible.

Hope above advice is helpful for you.

Have a nice day!

BR,

Weidong

0 Kudos