Timer & I2C write operation problem with i.MX6Q SabreSD kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Timer & I2C write operation problem with i.MX6Q SabreSD kit

2,242件の閲覧回数
Steve2k
Contributor I

Hi everyone. I'm a beginner at embedded system & linux kernel, using i.MX6Q SabreSD kit for studying. When learing how to use Timer, I have a problem with I2C write operation.

- I have an I2C device driver, I setup a timer in probe() function to call my callback function (called "my_timer_callback") after 1 second:

setup_timer(&my_timer, my_timer_callback, 0);
mod_timer(&my_timer, jiffies + msecs_to_jiffies(1000));

- Inside my callback function, I send 1 byte to reset my I2C slave device & restart my Timer:

static void my_timer_callback(unsigned long data)
{
     printk(KERN_INFO "----> %s\n", __func__);
     i2c_smbus_write_byte_data(my_i2c_client, 0x00, 0x00);
     mod_timer(&my_timer, jiffies + msecs_to_jiffies(1000));
}

- When I boot up the kit with new kernel image, the booting is error & log in minicom looks like this:

...

----> my_timer_callback                                               

clk_enable cannot be called in an interrupt context                     

[<c00509e4>] (unwind_backtrace+0x0/0x138) from [<c006b408>] (clk_enable+0x88/0x)

[<c006b408>] (clk_enable+0x88/0xa0) from [<c03c3fa8>] (i2c_imx_xfer+0x6c/0x75c)

[<c03c3fa8>] (i2c_imx_xfer+0x6c/0x75c) from [<c03c19cc>] (i2c_transfer+0xc8/0x1)

[<c03c19cc>] (i2c_transfer+0xc8/0x148) from [<c03c1d80>] (i2c_smbus_xfer+0x298/)

[<c03c1d80>] (i2c_smbus_xfer+0x298/0x564) from [<c03c22fc>] (i2c_smbus_write_by)

[<c03c22fc>] (i2c_smbus_write_byte_data+0x40/0x48) from [<c040335c>] (my_timer_)

[<c040335c>] (my_timer_callback+0x68/0xa4) from [<c009812c>] (run_timer_softirq)

[<c009812c>] (run_timer_softirq+0x134/0x3e4) from [<c0090478>] (__do_softirq+0x)

[<c0090478>] (__do_softirq+0xc8/0x25c) from [<c0090ac0>] (irq_exit+0x98/0xa0)

[<c0090ac0>] (irq_exit+0x98/0xa0) from [<c00431b4>] (do_local_timer+0x70/0x90)

[<c00431b4>] (do_local_timer+0x70/0x90) from [<c004934c>] (__irq_svc+0x4c/0xe8)

Exception stack(0xe6037e28 to 0xe6037e70)                                

7e20:                   e72f9c18 20000113 000025ed 00000000 e72f9800 e72f99d4

7e40: e72f9b40 e72f9c18 20000113 00000000 00000000 00000000 00000004 e6037e70

7e60: c043152c c06403e0 40000113 ffffffff                                

[<c004934c>] (__irq_svc+0x4c/0xe8) from [<c06403e0>] (_raw_spin_unlock_irqresto)

[<c06403e0>] (_raw_spin_unlock_irqrestore+0x18/0x40) from [<c043152c>] (sdhci_s)

[<c043152c>] (sdhci_set_ios+0x284/0x5ec) from [<c0420130>] (mmc_set_bus_mode+0x)

[<c0420130>] (mmc_set_bus_mode+0x3c/0x9c) from [<c0426dfc>] (mmc_sdio_init_card)

[<c0426dfc>] (mmc_sdio_init_card+0x438/0x570) from [<c0427398>] (mmc_attach_sdi)

[<c0427398>] (mmc_attach_sdio+0x94/0x368) from [<c0420ee8>] (mmc_rescan+0x24c/0)

[<c0420ee8>] (mmc_rescan+0x24c/0x2ac) from [<c00a3f5c>] (process_one_work+0x12c)

[<c00a3f5c>] (process_one_work+0x12c/0x494) from [<c00a4434>] (worker_thread+0x)

[<c00a4434>] (worker_thread+0x170/0x3cc) from [<c00a8528>] (kthread+0x80/0x88)

[<c00a8528>] (kthread+0x80/0x88) from [<c004a408>] (kernel_thread_exit+0x0/0x8)

kernel BUG at arch/arm/plat-mxc/clock.c:101!                             

Unable to handle kernel NULL pointer dereference at virtual address 00000000

pgd = c0004000                                                           

[00000000] *pgd=00000000                                                 

Internal error: Oops: 805 [#1] PREEMPT SMP                               

Modules linked in:                                                       

CPU: 0    Tainted: G        W    (3.0.35-g582b0a0-dirty #229)            

PC is at __bug+0x1c/0x28                                                 

LR is at __bug+0x18/0x28                                                 

pc : [<c004cfec>]    lr : [<c004cfe8>]    psr: 20000113                  

sp : e6037c28  ip : 00000000  fp : 00000001                              

r10: 00000001  r9 : ffff8c93  r8 : e6037ca8                              

r7 : c08dffe8  r6 : 00000001  r5 : e6037ca8  r4 : c08896f0               

r3 : 00000000  r2 : c089741c  r1 : 60000193  r0 : 00000033               

Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment kernel      

Control: 10c53c7d  Table: 1000404a  DAC: 00000015                        

                                                                         

PC: 0xc004cf6c:                                                          

cf6c  e1a04000 e24dd010 e590003c eb01c3bb e3500000 0594003c 0a00000d e2841034

cf8c  e594002c e891000e e88d000f ea000003 e59d000c eb01c3b1 e3500000 0a000006

cfac  e1a0000d eb000d34 e3500000 aafffff7 e3a00000 e28dd010 e8bd8010 e59d000c

cfcc  eafffffb e92d4008 e1a03000 e1a02001 e59f0010 e1a01003 eb17b2ab e3a03000

cfec  e5833000 eafffffe c076de8c e30d0ea8 e30012e1 e92d4008 e34c0076 ebfffff0

d00c  e1a01000 e30d0ec0 e92d4008 e34c0076 eb17b29d e30d0ea8 e30012c5 e34c0076

d02c  ebffffe7 e92d4008 e1a02000 e1a03001 e30d0ee0 e1a0100e e34c0076 eb17b292

d04c  e30d0ea8 e3001299 e34c0076 ebffffdc e92d4ff0 e24dd06c e1a06002 e1a08000

                                                                         

LR: 0xc004cf68:                                                          

cf68  e92d4010 e1a04000 e24dd010 e590003c eb01c3bb e3500000 0594003c 0a00000d

cf88  e2841034 e594002c e891000e e88d000f ea000003 e59d000c eb01c3b1 e3500000

cfa8  0a000006 e1a0000d eb000d34 e3500000 aafffff7 e3a00000 e28dd010 e8bd8010

cfc8  e59d000c eafffffb e92d4008 e1a03000 e1a02001 e59f0010 e1a01003 eb17b2ab

cfe8  e3a03000 e5833000 eafffffe c076de8c e30d0ea8 e30012e1 e92d4008 e34c0076

d008  ebfffff0 e1a01000 e30d0ec0 e92d4008 e34c0076 eb17b29d e30d0ea8 e30012c5

d028  e34c0076 ebffffe7 e92d4008 e1a02000 e1a03001 e30d0ee0 e1a0100e e34c0076

d048  eb17b292 e30d0ea8 e3001299 e34c0076 ebffffdc e92d4ff0 e24dd06c e1a06002

...

Please, help me to solve this problem. Thanks.

ラベル(2)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,670件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

The hint is the very first message of your log "clk_enable cannot be called in an interrupt context".

So you need to move the clk_enable() to some other place which is not in interrupt context.

Regards,

Fabio Estevam

0 件の賞賛
返信

1,670件の閲覧回数
Steve2k
Contributor I

Hi Fabio,

I think I've found the reason for this problem. I'll find another solutions supported by Linux kernel.

Thanks for your reply.

0 件の賞賛
返信