Time needed for ROM boot loader to start secondary boot loader in i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Time needed for ROM boot loader to start secondary boot loader in i.MX6

1,546件の閲覧回数
krishnanp
Contributor III

Greetings,

I have  board  based on i.MX6 and configured  with PARALLEL NOR  (EIM) as the boot device.

XTALOSC =24 MHZ and the data width of NOR is 16.

As per RM  below are the cloks at  boot time.

clocks.png

My question is ,

After the  power good signal, how much time does it take to run the first instruction of a secondary boot loader (considering BT_FREQ=0)?

XTALOSC =24 MHZ, System PLL = 792

NOR  DATA Width = 16.

NOR  ADDR Width = 25.

Thanks for your heads up.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,274件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Krishnan

please look below

ROM Code Boot Time Measurements

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信