Ti DS90UB947/948 Linux Driver for I.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ti DS90UB947/948 Linux Driver for I.MX6

1,749 Views
2479420618
Contributor II

Imx6 can output lvds direct.But the lvds-wire is too  expensive to buy. So they can cannect ds90ub947 serializer to applied in automotive instrumentation. By the way, it need a ds90ub948 deserializer in the remote which cannect a lvds displayer.

pastedImage_1.png

The attachment is the driver of ds90ub947/948 for linux.It can  support linux 3.10 and above.It was verified working on linux 3.10.53 and imx6q.

The attachment list:

ds90ub947.c

ds90ub947.h

readme.txt

You can follow the readme to use it.

This driver was barely in embryo.You should modify it according to your application.

Sometime, it very looks like the ds90ub913/914 and max9286/96705.

0 Kudos
Reply
1 Reply

1,090 Views
albert_zhang
Contributor II

Hello Zhongmiao,

I think your problem has been solved, so you just connect the I2C wires, and you didn't connect LVDS wires?