Hi @nxp
Can one give any reference link, how we can integrate battery charger with imx8mp.
With reference to imx part which things need to be taken care and configured.
BATTERY-MANAGEMENT-CONTROL
The issue is when battery is low, when we give power to the system it reboots for 4 to 5 time to get into system on.
What changes are required to make power flow directly from the power adopter to boot the system in one boot, even battery is low.
Hello,
This sounds like an issue in the output voltage of the battery charger.
Did you measure the output voltage?
Was it stable and under the operating range?
You may change the voltage threshold to detect a low battery voltage in your IC and avoid this issue; the output voltage could be close the minimum input voltage in i.MX side and any variation below this range could cause the reboot issue.
Best regards.