Throwing UART

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Throwing UART

跳至解决方案
1,563 次查看
aermakov
Contributor II

I am using iMX6ULL, and I have a question.

Is it possible to throw some functionality (e.g. UART) from one pin to another?

I need to have UART port, but in some cases this UART should be switched to external device and is no longer needed to me. Is there such a functionality?

标签 (1)
0 项奖励
回复
1 解答
1,420 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Alexey Ermakov,

You cannot change the device tree from one to another once the device tree has been loaded. However, you may change the registers that setup the muxing alternatives directly while the system is running.

On using the pad as an analog switch that would not be feasible due to the way the pads work. You can see more details on how the pads work on the product documentation, but the muxing options have also limitations on whether pins can be input/output or may also be fixed.

My apologies for the inconvenience!

Regards,

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,421 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Alexey Ermakov,

You cannot change the device tree from one to another once the device tree has been loaded. However, you may change the registers that setup the muxing alternatives directly while the system is running.

On using the pad as an analog switch that would not be feasible due to the way the pads work. You can see more details on how the pads work on the product documentation, but the muxing options have also limitations on whether pins can be input/output or may also be fixed.

My apologies for the inconvenience!

Regards,

0 项奖励
回复
1,420 次查看
aermakov
Contributor II

Actualy I want use pads as analog switch, such as NX3DV2567GU, for example

0 项奖励
回复