Three camera inputs for i.MX6Quad

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Three camera inputs for i.MX6Quad

ソリューションへジャンプ
1,493件の閲覧回数
yuuki
Senior Contributor II

Dear all,

We would like to connect three cameras to i.MX6.
(CSI Parallel port 2ch + MIPI-CSI port 1ch)

According to i.MX 6 Series Firmware Guide, MIPI and parallel seem to be exclusive.

i.MX 6 Series Firmware Guide Rev.0:
- 21.5 IOMUX pin mapping
- Table 21-4. Camera interface mode setting

Can three ports be inputted simultaneously?
If so, Could you teach the value of Bit19-20 of IOMUXC_GPR1 register which should be set up?

Best Regards,
Yuuki

ラベル(1)
1 解決策
1,230件の閲覧回数
Yuri
NXP Employee
NXP Employee

It is possible to connect three cams to i.MX6.

You may look at Figure 19-1 (CSI2IPU gasket connectivity) of the i.MX6 DQ Reference Manual.

MIPI_CSI.jpg


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,231件の閲覧回数
Yuri
NXP Employee
NXP Employee

It is possible to connect three cams to i.MX6.

You may look at Figure 19-1 (CSI2IPU gasket connectivity) of the i.MX6 DQ Reference Manual.

MIPI_CSI.jpg


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信