The vxworks BSP packages support for the i.MX serious

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The vxworks BSP packages support for the i.MX serious

585 Views
bratzhang
Contributor II

Dear Sir:

     Could NXP can support the BSP packages based on the vxworks of the i.MX serious such as i.MX28, i.MX6 etc..?

Labels (2)
0 Kudos
1 Reply

375 Views
Yuri
NXP Employee
NXP Employee

Hello,

  NXP does not support VxWorks directly. Please apply to Wind River.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos