Hi:
I am trying to U-boot the Linux Kernel(uImage-3.10-ts-armv7l) from the SD card.
But it hangs up after the "Verifying Checksum. . .OK".
Here are the settings I put in the boot:
bootargs=console=ttymxc0,115200 ip=dhcp root=/dev/mmcblk0p1 rw rootwait
bootcmd=ext2load mmc 0:1 ${fdt_addr} boot/uImage; ext2load mmc 0:1 ${loadaddr} boot/wandboard_solo.dtb; bootm ${fdt_addr} - ${loadaddr}
Here is the output from the booting:
CPU: Freescale i.MX6SOLO rev1.1 at 792 MHz
Reset cause: POR
Board: Wandboard
I2C: ready
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
auto-detected panel HDMI
Display: HDMI (1024x768)
In: serial
Out: serial
Err: serial
Net: FEC [PRIME]
Hit any key to stop autoboot: 0
5610720 bytes read in 389 ms (13.8 MiB/s)
44116 bytes read in 128 ms (335.9 KiB/s)
## Booting kernel from Legacy Image at 18000000 ...
Image Name: Linux-3.10.53-ts-armv7l-1.1.0_ga
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5610656 Bytes = 5.4 MiB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
Could you help me on fixing that?
Thank you.