The start up of the Linux kernel stuck after the Verifying Checksum

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The start up of the Linux kernel stuck after the Verifying Checksum

663 Views
jianyuanma
Contributor I

Hi:

I am trying to U-boot the Linux Kernel(uImage-3.10-ts-armv7l) from the SD card.

But it hangs up after the "Verifying Checksum. . .OK".

Here are the settings I put in the boot:

   bootargs=console=ttymxc0,115200 ip=dhcp root=/dev/mmcblk0p1 rw rootwait

   bootcmd=ext2load mmc 0:1 ${fdt_addr} boot/uImage; ext2load mmc 0:1 ${loadaddr} boot/wandboard_solo.dtb; bootm ${fdt_addr} - ${loadaddr}

Here is the output from the booting:

CPU: Freescale i.MX6SOLO rev1.1 at 792 MHz
Reset cause: POR
Board: Wandboard
I2C: ready
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
auto-detected panel HDMI
Display: HDMI (1024x768)
In: serial
Out: serial
Err: serial
Net: FEC [PRIME]
Hit any key to stop autoboot: 0
5610720 bytes read in 389 ms (13.8 MiB/s)
44116 bytes read in 128 ms (335.9 KiB/s)
## Booting kernel from Legacy Image at 18000000 ...
    Image Name: Linux-3.10.53-ts-armv7l-1.1.0_ga
    Image Type: ARM Linux Kernel Image (uncompressed)
    Data Size: 5610656 Bytes = 5.4 MiB
    Load Address: 10008000
    Entry Point: 10008000
    Verifying Checksum ... OK

Could you help me on fixing that?

Thank you.

0 Kudos
Reply
1 Reply

566 Views
joanxie
NXP TechSupport
NXP TechSupport

did  you program the image(uboot and kernel image) to sd card by mfgtool successfully? or you just download the uboot ?

0 Kudos
Reply