The size difference between IMX8MM and IMX8MN file system in Yocto L5.4.70

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The size difference between IMX8MM and IMX8MN file system in Yocto L5.4.70

1,428 次查看
joshua_jhan
Contributor III

Why the imx8m mini and imx8m nano on the same yocto version, the file system size difference?

In Yocto 5.4.70, the 8M mini using "df -h" the /dev/root used size is 1.5G,

but 8M nano is 2.1G.

our custom board the eMMC size only 4G, This situation will make it can't to flash image to eMMC on nano

标签 (1)
0 项奖励
回复
1 回复

1,412 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

The imx8m mini and imx8m nano are different, so the file system file size is not the same. For 4G emmc is not enough. Here you can try to use larger sd card if your board support it.

 

0 项奖励
回复