The size difference between IMX8MM and IMX8MN file system in Yocto L5.4.70

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The size difference between IMX8MM and IMX8MN file system in Yocto L5.4.70

1,290件の閲覧回数
joshua_jhan
Contributor III

Why the imx8m mini and imx8m nano on the same yocto version, the file system size difference?

In Yocto 5.4.70, the 8M mini using "df -h" the /dev/root used size is 1.5G,

but 8M nano is 2.1G.

our custom board the eMMC size only 4G, This situation will make it can't to flash image to eMMC on nano

ラベル(1)
0 件の賞賛
返信
1 返信

1,274件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

The imx8m mini and imx8m nano are different, so the file system file size is not the same. For 4G emmc is not enough. Here you can try to use larger sd card if your board support it.

 

0 件の賞賛
返信