The relation between ARM Cortex A53 64-bit and LPDDR4 16-bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The relation between ARM Cortex A53 64-bit and LPDDR4 16-bit

1,309 Views
nissim
Contributor II

Dear all, 

This question refers to the I.MX8 nano which is based on ARM Cortex A-53.

I would like to get a better understanding regarding the relation between the core (ARM Cortex A53 64-bit) and the external memory LPDDR4 from performance perspective.

According to i.MX 8M Nano Applications Processor Reference Manual document (Document Number: IMX8MNRM

Rev. 0, 12/2019), the DRAM controller and PHY includes: 

• LPDDR4-3200, DDR4-2400, and DDR3L-1600 in Non-POP BGA package
• 16-bit DRAM interface
• 800MHz 64-bit AXI bus

Let's assume that the external memory is an LPDDR4-3200 16-bit wide (transfer rate of 3200 MT/s --> 1.6GHz I/O bus clock). Taking into account that the external memory is DDR it means that the memory can handle 32-bits in one clock. Both AXI Bus and the A53 are 64-bit wide. However the frequency of the AXI bus is half (800MHz) of the frequency of the A53(1.5GHz).

If all of the above is correct, this architecture may lead to latency and performance issues. isn't it?

In addition, according to ARM documentation the The A53 L2 memory system interfaces to the external memory is 128-bits wide. how does it match to the fact the the AXI bus is 64-bits wide? 

Thanks,

Nissim.

Labels (2)
2 Replies

1,214 Views
mrudangshelat1
Senior Contributor II

Hi Nissim,

It is possible to achieve 3200MT/s using AXIS Bus.

Axis bus has 800MHz x 64bit = 51200 Mb/s

And LPDDR4 has 1600MHZ x 2 (DDR) x 16bit = 51200 Mb/s.

So there will not be any latency issue. If it is there then it can be handled by DDRC buffer as said by yuri.

Regards,

Mrudang

1,214 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Internal details of i.MX8Mn are not provided. Nevertheless, because of internal DDRC buffer(s)

it is possible to avoid performance issues.

Regards,

Yuri.