Hi,all
we are using imx8mm for H264 encoding, system information is as bellow:
CPU: MIMX8MM6DVTLZAA
software version: imx-4.14.98-2.0.0_ga.xml
vpu:====== VPUENC: 4.4.5 build on Oct 30 2019 12:04:50. ======
wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Sep 24 2021 08:24:44) vpulib: 1.1.1 firmware: 1.1.1.65535
Issues describe:
If we use the CBR mode, The output bit rate fluctuates by approximately 20%.
but in the VBR mode, The output bit rate fluctuates about 30k~30M (1080p/60fps, H264 encoding);
however, we test another solution, its output bit rate fluctuates about 30k~5M (most time is 4M);
so our quetsion is: is it possible to optimize MIMX8MM vpu for its VBR mode? can we make it's output bit rate fluctuates from 30k~30M to 30k~5M in VBR mode(1080p/60fps, H264 encoding)? anyother update? or give us some suggetion, thanks.
Looking forward to your reply